You are here: Getting Started > Advanced Project Creation > Add and Configure Drive > AKD Setup Wizard

AKD Setup Wizard...

The wizard allows you to configure drives once the following conditions have been met:

You then have access to the AKD parameters that are used when the drive is running.

AKD Setup Wizard

Figure 4-32: AKD Setup Wizard

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™